Develop a localized event logger
    Create an even logger that displays the interface in the language of a currently logged-in user.
Application example - English

Application example - Italian

     NOTE: 
    
Download a sample project:
 LocalizedEventLogger.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback