Create an event logger
    Create a logger that monitors the current temperature.
- InProject view, right-clickLoggersand select .
- Configure events:- InProperties, next toEvent configurations, select. 
- SetListen subtreetoFalse.
- Set theEvent typetoAlarmConditionType.
- InProperties, double-clickEventLogger1
- In the editor, select these variables:- .
- .
- .
- .
- .
- .
 
- In the editor, selectApply.
 
- Create a dynamic link betweenDatabaseand .For more information about dynamic links, see Create dynamic links.
Provide Feedback