Create a key value converter
    Create a converter that changes Boolean values into localized text.
- InProject view, right-clickConvertersand select .
- Double-click the converter.
- In the editor, set the following values:KeysBooleanValuesStringTrueTrueFalseFalseFor more information about dynamic links, see Create dynamic links.
Provide Feedback