Manage file and resource paths
    The 
ResourceURI
 static C# class represents the path (URI) of a file or resource inside or outside the project. 
     TIP: 
    The 
ResourceURI
 class represents the same type of data for the variables. For example, the Path
 property of an Image
 object.ResourceURI object properties
      
  ResourceURI
 object properties| Properties | Data type | Description | 
|---|---|---|
| URIType | URIType | The path type of the path contained:
                   
 | 
| ProjectRelativePath | string | The relative path of a file in relation to the  ProjectFilesfolder. | 
| ApplicationRelativePath | string | The relative path of a file in relation to the  ApplicationFilesfolder. | 
| AbsoluteFilePath | string | The absolute path of a file external to the project. | 
| URI | string | The absolute path of a generic resource. | 
| URIType | ProjectRelativePath | ApplicationRelativePath | AbsoluteFilePath | URI | 
|---|---|---|---|---|
| URI | - | - | - | URI (for example, a URL HTTP) | 
| ProjectRelative | Relative path to the  ProjectFilesfolder | - | - | Absolute path | 
| ApplicationRelative | - | Relative path in relation to the  ApplicationFilesfolder | - | Absolute path | 
| AbsoluteFilePath | - | - | Absolute path | Absolute path | 
Provide Feedback