ResourceURI.FromAbsoluteFilePath(path)
    Returns a C# object of the 
ResourceURI
 type, with the URIType
 of AbsoluteFilePath
 that contains an absolute path to a file.static ResourceUri FromAbsoluteFilePath(stringpath);
Arguments
      - path(string)
- An absolute path to a file.
Returns
      - ResourceURI
- A C# object that contains the path indicated in the argument.
Example
      The following example shows an API that returns a C# 
applicationRelativeResourceURI
 object of theResourceURI
 type that contains the relative path C:\Users\Username\Desktop\Text1.txt
.var applicationRelativeResourceUri = ResourceUri.FromAbsolutePath("C:\Users\Username\Desktop\Text1.txt");
Provide Feedback