ResourceURI.FromURI(uri)
    Returns a C# object of the 
ResourceURI
 type, with the URIType
 type pf URI
 and that contains an absolute path to a generic resource.Arguments
      - uri(string)
- An absolute path of a generic resource, usually a network path or a website address.
Returns
      - ResourceURI
- A C# object that contains the path indicated in the argument.
Example
      Below is an example in which the API returns a C # website object of the 
ResourceURI
 type that contains the https://www.rockwellautomation.com/
 URL.
        var website = ResourceURI.FromURI("https://www.rockwellautomation.com/");
Provide Feedback