Import or export recipes at runtime
    Use the RecipeImportExport NetLogic to import recipes from a 
CSV
 file or export recipes to a CSV
 file at runtime.Prerequisites
- To import or export recipes at runtime
- From the toolbar, select.Template Libraries
- InLibraries:- SelectScripts.
- From the right pane, dragRecipes Import Exportto a folder inProject view.DragRecipes Import Exportto theModelfolder.
- SelectClose.
 
- InProject view, select theRecipeImportExportobject.
- InProperties:- In theRecipeSchemaproperty, select the recipe schema of the reference object.
- In theCSVFile, enter the full path of theCSVfile to import or export.C:\temp\export_recipes.csvNOTE: The fields of theCSVfile to import must be the same as the database columns.
- In theCSVSeparatorproperty, set the CSV delimiter.
- To delimit the fields with quotation marks in theCSVfile, set theWrapFieldsproperty toTrue.
 
- Configure the buttons to trigger import or export:- Add a Button object in a container and associate its MouseClick Event with the NetLogic Import method.
- Add a Button object in a container and associate its MouseClick Event with the NetLogic Export method.
 For more information, see Button and Add a method to an existing event.
Provide Feedback