Configure a recipes editor
    You add a recipes editor widget by selecting it from the template libraries and editing its properties.
     TIP: 
    You can develop your own recipes management solution. For more information, see Recipes editor customization.
Prerequisites
- To configure a recipes editor
- From the toolbar, select.Template Libraries
- InTemplate Libraries:- SelectWidgets.
- DragRecipes Editorto theUIfolder inProject view.
- SelectClose.
 
- InProject view, double-clickRecipesEditor.The widget preview displays in the editor.
- InProperties, in theRecipeSchemaproperty, select aRecipe Schemaobject.
- InProject view, automatically configure the graphical objects and dynamic links used to assign values to ingredients at runtime by right-clicking theRecipesEditorobject and selectingExecute Setup.
The ingredients list appears in the widget.
Do any of the following:
        
Provide Feedback