Manage recipes at runtime
    Use the recipes editor widget to store a new recipe, to delete an existing recipe, or to apply a recipe on the controller.
When the user creates, edits, or loads a recipe from the database at runtime, an alias to the 
    
    
Edit model
 node is automatically created in the root project node. The alias node has the same name as the recipe schema it refers to. Until the node is saved, deleted, or sent to the controller, it contains a temporary copy of the created, edited, or loaded recipe data.
      
     IMPORTANT: 
    If the 
FTOptixApplication
 execution stops, the Edit model
 node and its data are deleted.- To manage recipes at runtime
- To store a new recipe:- Edit the values of the ingredients.
- In the recipe list, enter a name for the recipe.
- SelectSave.
 
- To delete a recipe, select a recipe and selectDelete.
- To apply a recipe on the controller:- Select a recipe.Recipe ingredients values display.
- SelectApply.In the right column, ingredients values loaded to the controller display.
- To change the values of the ingredients on the controller, edit the values, selectSaveand selectApply.The values of the ingredients on the controller update in the right column.
 
Provide Feedback