Presentation engines
    A presentation engine object displays UI elements at runtime.
Native presentation engine
      Use the Native presentation engine for typical HMI applications that run on targets with an
        operator panel. There can be only one Native presentation engine in a project.
When you run a project, an interactive session generates and authenticates with the
        starting user.
You can change the current user in an interactive session. Based on the user and logic created, the interface can change dynamically in the same session.
        
    
    
     TIP: 
    To specify the user, see Global methods for user authentication or Session activity log and audit.
Web presentation engine
      Use a Web presentation engine to make a web user interface available to multiple users who
        connect from different web browsers. Web presentation engines are compatible with HMI
        applications that run on target devices equipped with an operator panel and with devices
        that do not have a dedicated administration interface. There can be only one Web
        presentation engine in a project.
     TIP: 
    
Due to security reasons, to view websites with self-signed SSL certificates inside a
          WebBrowser object with the Web Presentation Engine, you must first open the website in
          another tab of the same browser and approve the certificate in that tab. You can then go
          to the WebUI tab and reload the page to display the self-signed SSL website. Only websites
          with a content security policy that allows embedding can open inside a WebBrowser on a
          WebUI session.  See Certificate errors.
When a user connects to the web server, an interactive session is generated for the
        authenticated user. The same user can generate additional interactive sessions by accessing
        the project from multiple devices. Each session creates a start window. See Sessions and locales.
     TIP: 
    Use the  variable to get the IP address of the client. Create dynamic links to use the
        client IP address in the application logic. For example, display different graphic objects
        to clients connecting from specific IP addresses. For more information, see Dynamic links and Aliases.
     TIP: 
    Web presentation engine can only load files from the
        project directory (
%PROJECTDIR%
). This applies to any object in the
        project that can load files, including image, web browser, and PDF viewer objects.SVGs in presentation engines
      To use an SVG image that renders consistently between the WebPresentation Engine and the NativePresentation Engine, you must define a height and width attribute for the SVG element within the image file. 
For example:
<svg xmlns:xlink="http://www.w3.org/1999/xlink" height="100" width="100" xmlns="http://www.w3.org/2000/svg"> <rect width="100" height="100" style="fill:rgb(0,0,255)"/> </svg>
Session
      Both the native presentation engine and web presentation engine expose a session type
        pointer. To read or modify session nodes, use the 
{Session}
 alias
        instead. For more information, see Built-in aliases.SVG
    
Provide Feedback