Built-in aliases
    The built-in aliases include Window, RecipeSchema, and Session aliases.
Window aliases
      You can use the  alias to reference to the application window properties and graphical objects that are present in that window.
RecipeSchema aliases
      At design time, the project root node contains an alias for each 
    
    
RecipeSchema
 instance in the project. This alias has the same name as the related RecipeSchema
 object. The project also contains a Panel loaders
 object. Access the RecipeSchema
 aliases from any node that have the same BrowseName as the corresponding objects in the project. For example, a PanelLoader1
 alias is generated for a PanelLoader1
 object.
        
     TIP: 
    Aliases for 
Recipe Schema
 objects are created inside the project root node.Session aliases
      The  alias points to the 
Session
 node that exists only at runtime. This alias contains several nodes that have values based on the user and session locale. At design time. this alias is always available for graphic objects and types.window alias
recipeschema alias
session alias
default aliases
    
Provide Feedback