Certificate errors
    Certificate errors may display when using the web browser object.
Certificate errors that are ignored at runtime when 
Ignore invalid CA
          errors
 is set to True
. For more information, see Configure a web browser.| Error | Description | 
|---|---|
| CertificateAuthorityInvalid  | Certificate not signed by a trusted CA  | 
Certificate errors listed in 
Certificate error
. To ignore the
        errors, select Accept the risk and continue
 at runtime.| Error | Description | 
|---|---|
| SslPinnedKeyNotInCertificateChain | Certificate does not match the built-in public keys pinned for the host name | 
| CertificateCommonNameInvalid | Certificate common name does not match host name | 
| CertificateDateInvalid | Certificate is not valid at the current date and time | 
| CertificateAuthorityInvalid | Certificate not signed by a trusted CA | 
| CertificateContainsErrors | Certificate contains errors | 
| CertificateNoRevocationMechanism | Unable to determine if the certificate is revoked | 
| CertificateUnableToCheckRevocation | Unable to get revocation information for the certificate | 
| CertificateRevoked | Revoked certificate | 
| CertificateInvalid | Invalid certificate | 
| CertificateWeakSignatureAlgorithm | Certificate signed with a weak signature algorithm | 
| CertificateNonUniqueName | Certificate host name is not unique | 
| CertificateWeakKey | Certificate contains a weak key | 
| CertificateNameConstraintViolation | Certificate claimed DNS names violate name constraints | 
| CertificateValidityTooLong | Too long certificate validity period | 
| CertificateTransparencyRequired | Unable to get required certificate transparency information from the server | 
| CertificateKnownInterceptionBlocked | Certificate known for interception by an entity other than the device owner | 
certificate
    
Provide Feedback