Manage graphic objects
    Create, edit, move, and delete graphic object types and instances.
Object types and object instances
      Any object that you create in the default 
    
    
UI
 folder or a subfolder of the UI
 folder is automatically configured as a type. See Create a graphic object type.
        
     TIP: 
    Types are available in 
Type view
 in the UI
 folder.To add graphic objects to 
FactoryTalk Optix Applications
, create object instances from object types. See Create a graphic object from a type.Objects management
      Use 
Project view
 and the editor to duplicate, rename, and edit the properties of graphic objects.
        Objects interactivity
      By editing graphic object properties, you can make the object movable or animate the object. For more information, see:
        
Objects protection
      In 
Project view
, lock graphic objects to prevent other FactoryTalk Optix Studio
 users from editing the object children at design time. You can set a password required to unlock the object as an additional layer of security.
        Provide Feedback