Common properties
    The available properties of UI objects depend on the selected object.
     NOTE: 
    
For any property that has a non-specific numeric value, the value Auto is equal to -1. If you double-click Auto in the property, -1 appears. If you enter -1 in the property, the value displays Auto.  
| Property | Description | Values | 
|---|---|---|
| Name | The name of the object. | String value. | 
| Type | The type of the object. | Uneditable value. | 
Appearance
      
  | Property | Description | Values | 
|---|---|---|
| Visible | Visibility of object at runtime | 
 | 
| Enabled | Whether the object allows user interaction at runtime | 
 | 
| Opacity | Transparency of the object | Numeric values from 0-100 with 0 making the object transparent. | 
| Blink | Allows the object to blink periodically, ignored when the object is not visible | 
 | 
| Rotation | Rotation of the object around the center point | Numeric values. Positive values indicate clockwise rotation in degrees. | 
| Border color | Color of the border of the object | Any selected or entered color of the linked tag. | 
| Fill color | Fill color of the object | Any selected or entered color of the linked tag. | 
| Border thickness | Thickness of the object border in pixels | Numeric value. | 
| Corner radius | Curvature of the corners of a rectangle in pixels | Numeric value. | 
| Hit test visible | Whether the user can select the object to perform event methods at runtime | 
 | 
| Move target | Determines if the object or ancestor object is movable at runtime. | 
 | 
Size and layout
      
  | Property | Description | Values | 
|---|---|---|
| Horizontal alignment | Align selected objects horizontally in the window | 
 | 
| Vertical alignment | Align selected objects vertically in the window | 
 | 
| Width | Width of the object  | Numeric value in pixels | 
| Height | Height of the object | Numeric value in pixels | 
| Left margin | Distance, in pixels, between the left edge of the window and the left side of the object | Numeric value | 
| Top margin | Distance, in pixels, between the top of the window and the top of the object | Numeric value | 
| Right margin | Distance, in pixels, between the right edge of the window and the right side of the object | Numeric value | 
| Bottom margin | Distance, in pixels, between the bottom of the window and the bottom of the object | Numeric value | 
Provide Feedback