Graphic objects
    Use predefined graphic objects to add visual components to 
FactoryTalk Optix Applications
. Use presentation engines to display the application UI at runtime on different viewports.Predefined graphic objects
      FactoryTalk Optix Studio
 includes different categories of predefined graphic objects to add to your project. You can customize the predefined graphic objects by editing their properties and by creating, editing, and modifying style sheets. You can also create custom graphic object types.For more information, see Predefined graphic objects.
Graphic objects management
      In 
Project view
 and in the editor, create, duplicate, edit, and set properties of graphic object instances and graphic object types. For interface overview, see:
        
For procedures, see:
        
Provide Feedback