Editor
    Open the editor for the user interface by opening a container object.
Editor

|  Item |  Description | Icon | Description | 
|---|---|---|---|
|  | Tab of the open window or object  | ||
|  | Canvas that displays the open window or object  | ||
|  | Design area for the contents of the open window or object | ||
|  | Editor toolbar with icons and options that depend on the objects selected in the design area |  | Select. Select items in the design area. | 
| Rectangle. Draw a rectangle in the design area. | |||
| Ellipse. Draw an oval in the design area. | |||
| Line. Draw a line in the design area. | |||
|  | Polyline. Draw a polyline in the design area. | ||
|  | Send to back. Send the selected object to the back of the objects in the design area. | ||
|  | Send backward. Send the selected object back one object in the design area. | ||
|  | Bring forward. Bring the selected object forward one object in the design area. | ||
|  | Bring to front. Send the selected object to the front of the objects in the design area. | ||
|  | Left align group. Align the selected objects along the leftmost object. | ||
|  | Top align group. Align the selected objects along the highest object. | ||
|  | Right align group. Align the selected objects along the rightmost object. | ||
|  | Bottom align group. Align the selected objects along the lowest object. | ||
|  | Dock left. Anchor the selected objects on the left while maintaining margins. | ||
|  | Dock center. Anchor the selected objects vertically while centering the objects and resetting margins. | ||
|  | Dock right. Anchor the selected objects on the right while maintaining margins. | ||
|  | Dock left and right. Stretch the selected objects horizontally across the container. | ||
|  | Dock top. Anchor the selected objects at the top while maintaining margins. | ||
|  | Dock center. Anchor the selected objects horizontally while centering the objects and resetting margins. | ||
|  | Dock bottom. Anchor the selected objects at the bottom while maintaining margins. | ||
|  | Dock top and bottom. Stretch the selected objects vertically across the container. | ||
| Delete. Remove the selected object from the design area. | |||
|  | Select the language for the objects in the design area. | ||
|  | Select the zoom level for the design area. | ||
|  | Select options to specify the visibility, snap placement of objects, and size of the grid. | 
editor
    
Provide Feedback