Configure the editor grid
    Configure the grid in the editor to show or hide the grid, align objects in the grid, and size the grid.
- InProject view, double-click a container object, or select. The editor opens in a new tab. The editor opens in a new tab.
- In the editor toolbar, select. Grid settings Grid settings
- Select the option to configure the grid:- Grid Visible. Toggle showing the grid in the editor.
- Snap to grid. Align the edges of objects with the grid.
- Grid size. Specify the size of the grid in pixels.
 
grid
editor grid
    
Provide Feedback