Configure an FTP server
    - Install stable versions of the following NuGet packages:
- Configure the requiredFTPServerLogicscript parameters. See FTP Server configuration.
- Run theFTPServerLogicscript.
ftp server
    
Provide Feedback