NuGet packages
    Some library widgets and scripts require specific NuGet packages to be installed.
For more information about NuGet, see What is NuGet and what does it do? | Microsoft Docs.
     IMPORTANT: 
    
FactoryTalk Optix Studio
 supports only .NET libraries with the .NET Standard 8 destination
      framework. To debug FactoryTalk Optix Applications
 with Visual Studio®
 or Visual Studio Code®
, install .NET SDK.
     IMPORTANT: 
    
Rockwell Automation
        is not responsible for any third-party software, including but not limited to its
        performance, security, updates, or compatibility with our products. Any use of third-party
        software is at your own risk, and we do not provide support, warranties, or guarantees for
        such software. Users should refer to the respective third-party providers for assistance and
        licensing terms.Install NuGet packages in the code editor of your choice. See Install NuGet packages in Visual Studio and Install NuGet packages in Visual Studio Code.
nuget
    
Provide Feedback