FTP Server configuration
    You can enable a File Transfer Protocol (FTP) server in your 
FactoryTalk Optix Application
.The runtime script 
    
    
FTPServerLogic
 enables an FTP server within a FactoryTalk Optix Application
. The script is found in the Scripts
 category in Template Libraries
.
      
     IMPORTANT: 
    You should start and stop the server only by using the exported OPC UA methods: 
StartFtpServer
 and StopFtpServer
.Required packages
      You must install stable versions of the following required NuGet packages:
        
Required parameters
      The FTP server requires the following parameters to be configured:
| Parameter | Description | Configuration | 
|---|---|---|
| IPAddress | IP address assigned to the server.  | The default value is set to  127.0.0.1. | 
| Port | Port assigned to the FTP server, | The default value is  21. | 
| FilesystemRoot | FTP server exposes only a fraction of the local filesystem to client | On  OptixPanel, you can only set either: 
 | 
| MinimumPASVPort | Minimum port number for managing file listing and file transfer. | This value must be greater than the default  1024. | 
| MaximumPASVPort | Maximum port number for managing file listing or file transfer. | This value must be greater than  MinimumPASVPort. The default value for MaximumPASVPortis 1100. | 
| Username/Password | FTP Server login credentials | |
| ServerCertificateFile | Server public certificate file, according to standard X509v3 and with .der extension.  | It must be found in the  FTOptixApplication/ProjectFiles/PKI/Own/Certsdirectory. If specified, the private key must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certsdirectory. | 
| ServerPrivateKeyFile | Server private key file, with ASCII Base64 encoding and .pem extension.  | It must be found in the  FTOptixApplication/ProjectFiles/PKI/Own/Certsdirectory. If specified, the certificate must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certsdirectory. | 
| UseFtps | Determine protocol to use, FTP or FTPS.  | The FTP server is started/stopped via the  StartFtpServer/StopFtpServermethods. | 
FTP
server
nuget
    
Provide Feedback