Safety Project Configuration

Safety projects require additional configuration after you create the project. These topics describe how to configure your controller.
For a safety-enabled controller, the programming software creates a safety task and a safety program. A main Ladder Diagram safety routine that is called MainRoutine is also created within the safety program.
A red bar under the icon distinguishes safety programs and routines from standard project components in the Controller Organizer.
Safety Components
This image shows the Safety Task in a Logix Designer project's Tasks.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal