Paste a Safety Network Number
If you must apply a Safety Network Number to other controllers, you can copy and paste the SNN.
To paste a Safety Network Number, complete the following steps.
- On the Online toolbar, click the Controller Properties icon.
- On the Controller Properties dialog box, click the Safety tab.
- On the Safety tab, click the ellipse to the right of the Safety Network Number.

- On the Safety Network Number dialog box, click Paste and then OK.
- On the Controller Properties dialog box, click OK.
Provide Feedback