Automatic Assignment of Time-based Safety Network Number
When a new controller or device is created, a time-based SNN is automatically assigned.
- Devices that are created directly under the controller port default to having the same SNN as that port on the controller.
- For devices not directly under a controller port, subsequent new safety device additions to the sameCIP Safety™network are assigned the same SNN defined within the lowest address on thatCIP Safety™network.
The time-based format sets the SNN value as the date and time when the number was generated, according to the computer running the configuration software.
Time-based Format

Provide Feedback