A warning occurs when opening an application with single sign-on
When opening a local or network application, if only the current logged on
Windows
-linked account is added to the Runtime Security
accounts list, you may receive a warning message indicating that you do not have security privileges to access the application.This might be because the user account security setting has not taken effect yet. To resolve this problem, you should log off
FactoryTalk Administration Console
and log on again. To log off from FactoryTalk
, either:- Log offWindows
- Right-click theFactoryTalk Directorynotification icon in the system tray and selectLogin/Logoutto openLog On toand selectFactoryTalkLog Off.
- Go toRockwell Software >Log On toand selectFactoryTalkLog Off.
Provide Feedback