I don't know the password to a directory
If you are trying to configure a directory but you are being prompted for a password you don't have, this might be because you are upgrading from
FactoryTalk Automation Platform
version 2.00.In version 2.00, you had to create passwords for
FactoryTalk
administrator accounts in both the network directory and the local directory.To upgrade existing directories to
FactoryTalk Services Platform
version 2.10 or later, you must supply the original user name and password for the FactoryTalk
administrator accounts.- For theFactoryTalklocal directory, the original default user name was Administrator, and the password field was left blank.
- For theFactoryTalknetwork directory, the original default user name was Administrator, but you were prompted to provide a password.
If you cannot remember the password to an existing directory, you cannot access that directory. Contact
Rockwell Automation
Technical Support.Provide Feedback