FactoryTalk Directory event log (Diagnostics Viewer)

In a
FactoryTalk
-enabled automation system,
Rockwell Automation
software products monitor system activity and generate detailed diagnostic messages. Meanwhile,
FactoryTalk Diagnostics
collects these messages from all participating products throughout a distributed system and routes them to Local Logs (also called event logs) on each computer.
If you encounter a problem, you can review the events in the log that led up to the problem to assist in determining the cause. Or you can monitor the log to identify potential problems and take corrective action before a problem occurs.
To view messages logged to the Local Log, open the
FactoryTalk Diagnostics
Viewer
on the computer where the alarm server resides.
You can:
  • Open the
    Diagnostics Viewer
    from within
    FactoryTalk Administration Console
    or
    FactoryTalk View Studio
    . From the
    Tools
    menu, click
    FactoryTalk Diagnostics
    > Viewer
    .
  • Open the
    Diagnostics Viewer
    from the Windows Start menu:
    Start > All Programs > Rockwell Software >
    FactoryTalk
    Tools > Diagnostics Viewer
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal