Common ControlLogix event log entries
A large number of on the computer where the alarm server resides.
ControlLogix
event log entries are available for identifying the events that led up to a problem. Or you can monitor the log to identify potential problems. To view ControlLogix
messages logged to the local (event) log, open the FactoryTalk Diagnostics
ViewerProvide Feedback