Advance tab for FactoryTalk Linx device discovery
How do I open the dialog box?
Use one of the following methods:
- From theCommunication Setupeditor, right-click on the device shown at the root, and then clickProperties.
- From theCommunicationstab ofFactoryTalk Administration Console, right-click on the device shown at the root, and then clickProperties.
The
Advance
tab provides the configuration field to set maximum concurrent packets to browse bridged networks, the concurrent processors to upload extended properties, and the terminal file transfer communication packet size.Use the
FactoryTalk Linx
Advance tab when browsing an Ethernet subnet that is connected to the computer indirectly. Either through a USB interface, across a ControlLogix backplane, or across a Logix 5000
controller with multiple communication ports. Set the maximum concurrent packets specifies the number of simultaneous devices FactoryTalk Linx
will attempt to detect at any single time.- Setting this value higher will improve the rate thatFactoryTalk Linxdetects devices when the user is browsing the network, but could limit the number of communications connections through a device which can be utilized for other operations.
- Setting this value lower will reduce the likelihood that a network browse impacts other operations but will reduce the rate that devices are detected and presented in the topology tree.
Enter the maximum concurrent packets value to browse the bridged network when bridged devices are connected.
Provide Feedback