Advance settings for FactoryTalk Linx device discovery

The following are the settings on the
Advance
tab of the
Device Properties
dialog box.
Setting
Description
Maximum concurrent packets to browse bridged network
Specify the maximum concurrent packets value (the default value is 32, minimum value is 1, maximum value is 64).
Concurrent processors to upload extended properties
Specifies the concurrent processor threads to upload extended properties (the default value is 5, minimum value is 1, maximum value is 16)
Terminal file transfer communication packet size
Specify the packet size to communicate with the terminal (the default value is 2000).
Note
: Update this option to 1400 on a virtual machine to improve performance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal