Define system-wide alarm settings
Use the
General
tab in the System Settings Properties
dialog box to specify alarm settings that apply to all FactoryTalk
alarm servers in a FactoryTalk Directory
.To define system-wide alarm settings
- OpenFactoryTalk Administration ConsoleorFactoryTalk View Studio.
- In theFactoryTalkExplorer window, expandSystem > Policies > System Policies >.FactoryTalk Alarms and Events
- Double-clickSystem Settingsto open theSystem Settings Propertiesdialog box.
- In theHandle special eventsarea, select the check boxes to choose which events to send to the event log.
- In theBuffer events before sending to clientsarea specify the limits the alarm server will use to determine when to send buffered event data toFactoryTalk Alarms and Eventsclient objects.
- In theAssign alarm prioritiesarea specify integers for the lower limit in each priority range. You cannot leave gaps or have overlaps in the values specified.
- When finished with making changes, clickOKto close the dialog box and apply the settings.
Provide Feedback