System Settings Properties - General tab

How do I open the System Settings Properties dialog box?
  1. In the FactoryTalk Administration Console or FactoryTalk View Studio
    Explorer
    window, expand
    System > Policies > System Policies > FactoryTalk Alarms and Events
    .
  2. Double-click
    System Settings
    .
Use the
General
tab in the System Settings Properties dialog box to specify alarm settings that apply to all alarm servers in a
FactoryTalk Directory
.
The following table provides descriptions of these settings and how they can be used:
Setting
Description
Handle special events
The settings in this area determine which events are sent to the event log.
  • Send operator action audit messages to the alarm and event history log
FactoryTalk Alarms and Events
generates audit messages for operator actions, such as acknowledging or disabling alarms.
FactoryTalk
Audit events are always generated and can be routed to the
FactoryTalk
Audit Log and the Local Log of
FactoryTalk Diagnostics
.
Select this check box to generate tracking events for operator actions and send them to the alarm and event history log.
  • Send suppressed alarms to the alarm and event history log
Use this setting to configure whether changes in the alarm state for suppressed alarms are recorded in the alarm and event history log. This setting affects all alarm and event servers in a
FactoryTalk
system.
Select this check box to record suppressed alarm state changes in the alarm and event history log.
Clear this check box to prevent recording these changes in the log.
  • Only send changes in Quality for active alarms to the alarm history log
Use this setting to configure the way changes in alarm quality (faults) are recorded in the alarm and event history log:
Select this check box to send changes in quality for only active alarms to the alarm history log. This prevents the log from filling with non-critical events.
Clear this check box to send changes in quality for all alarms (active or otherwise) to the log.
Buffer events before sending to clients
The settings in this area determine when events are sent from the alarm server buffer to the
FactoryTalk Alarms and Events
client objects. When the system reaches either the event buffer size or event buffer time requirement defined in this area, all queued events are then sent to attached clients, such as the Alarm and Event Summary. Whichever of the two limits is reached first determines when queued events are sent to clients. System-wide settings for event buffering apply to all alarm servers defined in all applications in a
FactoryTalk Directory
.
  • Until x events have occurred
The number of events that alarm servers queue before sending the events on to attached clients. Set as a value between 1 and 100 (default is 10).
  • Or until x seconds have elapsed
The number of seconds that alarm servers queue events before sending the events on to attached clients. When the first event enters the queue, the queue 'timer' is started. When the time value is reached, the contents of the queue is sent to attached clients. Set as a value between 0.5 and 5.0 seconds (default is 0.5 seconds).
Assign alarm priorities
Settings in this area determine how the severity value of alarms are translated in priorities. Alarms and events can be assigned a particular severity value--an integer from 1 to 1000. Severity values are grouped into four priorities, corresponding to these four levels: Urgent, High, Medium, and Low. This makes it easier to filter and sort events and to distinguish among levels of urgency.
Define alarm priority settings by filling in the values in the
Low
column. You cannot leave gaps or overlaps in the settings.
The default alarm priority settings are:
  • Urgent priority - lower limit
    . Default severity value is 751.
  • High priority - lower limit
    . Default severity value is 501.
  • Medium priority - lower limit
    . Default severity value is 251.
  • Low priority - lower limit
    . Default severity value is 1.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal