Print events

You can print the contents of the Automatic Diagnostic Event Summary event list.
To print the contents of the event list
  1. On the toolbar, click the
    Print
    Diag_toolbar_printer button, or right-click an event and click
    Print
    .
  2. In the
    Print
    dialog box, select a printer type, and then choose the print range.
  3. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal