Find events
At runtime, operators can search for a text or numeric string in the event list portion of the Automatic Diagnostic Event Summary. Only the columns that are displayed in the event list are searched.
To find a text or numeric string in the event list
- On the toolbar, click theFind
button, or right-click an event and click
Find. - In theFind whatbox, type the text or numeric string you want to find.
- To search the events above the currently-selected event in the event list, clickUp. To search the events below the currently-selected event in the event list, clickDown.
- To search for a string that matches the case of the text in theFind whatbox, select theMatch casecheck box. To search for all matches, regardless of case, clear theMatch casecheck box.
- ClickFind next.
Provide Feedback