Alarm and Event Log Viewer Properties - General tab

How do I open the Alarm and Event Log Viewer Properties dialog box?
To open the
FactoryTalk Alarm and Event Log Viewer Properties
dialog box at design time:
  1. Open
    FactoryTalk View
    Studio.
  2. Add an
    Alarm and Event Log Viewer
    object to a graphic display.
  3. Right-click the Alarm and Event Log Viewer object and then click
    Properties
    .
Use the
General
tab in the Alarm and Event Log Viewer Properties dialog box at design time to change how information is displayed and how you interact with the information in the Alarm and Event Log Viewer at runtime.
The following table describes the settings available on the
General
tab and how they can be used:
Setting
Description
Alarm and event log
List of the alarm database names retrieved from the
System > Connections > Databases
folder in the FactoryTalk Directory. The first name in the list is selected when this page is presented unless an alarm database was previously selected by the designer. The selected alarm database is queried for historical data requested at runtime. Only one alarm database can be selected from the list.
Display report on startup
To display alarm and event information when the Alarm and Event Log Viewer opens, use the drop down list.
To open the Alarm and Event Log Viewer without querying the alarm database for historical data, clear this check box.
Allow details pane to be adjusted
To adjust the window height of the Details pane at runtime, select this check box.
Show
The check boxes in this area are used to control the display of interface elements in the Alarm and Event Log Viewer.
Horizontal grid lines
To show horizontal grid lines between rows in the event list, select this check box.
This is helpful especially when the Alarm and Event Log Viewer is very wide.
Vertical grid lines
To show vertical grid lines between columns in the event list, select this check box.
This is helpful especially when the columns are spaced closely together.
Details pane
To show the details pane, select this check box.
Toolbar
To show the toolbar, select this check box.
Status bar
To show the status bar at the bottom of the Alarm and Event Log Viewer, select this check box.
Tooltips
To show tooltips for the toolbar and status bar, select this check box.
Quality messages
To show messages of Quality Good or Quality Not Good in the event list, select this check box.
These messages will show when the alarm quality changes such as when a connection is lost or when it comes back to normal.
Border
To show the solid border line in the Alarm and Event Log Viewer, select this check box. To hide the solid border line in the Alarm and Event Log Viewer, clear this check box.
Icon style
Select an icon style to show.
Toolbar
The settings in this area change the appearance of the toolbar that is displayed at the top of the Alarm and Event Log Viewer.
If screen space is limited and operators can interact with the Alarm and Event Log Viewer using separate controls on a keypad terminal, you can hide the toolbar.
Text color
To select a color for the caption text on the buttons on the toolbar, click the color box.
Background color
To select a background color for the toolbar buttons, click the color box.
Icon size
To select a size for the icons on the toolbar, in the
Icon size
box, click the down arrow and make a selection.
Use larger icon sizes for touch-screen terminals.
Column headings
Use the settings in this area to change the appearance of the Event List displayed at the top of the Alarm and Event Log Viewer.
Text color
To select a color for the text in the column headings, click the color box.
Background color
To select a color for the background for the column headings, click the color box.
Row text
Use the settings in this area to change the appearance of the text in the rows of the events list at the top of the Alarm and Event Log Viewer.
Selection foreground color
To select a color for the text of selected items in the event list, click the color box.
Selection background color
To select a color for the background of selected items in the event list, click the color box.
Grid
The settings in this area change the appearance of the grid in the event list at the top of the Alarm and Event Log Viewer.
Line color
To select a color for the horizontal and vertical grid lines in the event list at the top of the Alarm and Event Log Viewer, click the color box.
Background color
To select a background color for the event list at the top of the Alarm and Event Log Viewer, click the color box.
Details pane
The settings in this area change the appearance of the information displayed in the details pane at the bottom of the Alarm and Event Log Viewer.
To keep the Details pane window height from being adjusted at runtime, clear this check box.
Text color
To select a color for the text displayed in the details pane, click the color box. Choose a color that contrasts well with the background color of the details pane.
Background color
To select a color for the background of the details pane, click the color box. Choose a color that contrasts well with the color of the text in the details pane.
Height
Type a value in percent for the size of the details pane relative to the size of the whole Alarm and Event Log Viewer object.
Fonts
The settings in this area change the font for text in the Alarm and Event Log Viewer.
Text font
To select a font for text presented in the Alarm and Event Log Viewer, click the
Browse
button and choose a font from the list.
Avoid fonts that are difficult to read.
Default print font
To select a default font for text that is sent to a printer, click the
Browse
button and choose a font from the list.
Make sure to match the font and font size to the printer and paper size used for printing reports.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal