Alarm and Event Log Viewer Properties - Toolbar tab
How do I open the Alarm and Event Log Viewer Properties dialog box?
To open the
FactoryTalk Alarm and Event Log Viewer Properties
dialog box at design time:- OpenFactoryTalk ViewStudio.
- Add anAlarm and Event Log Viewerobject to a graphic display.
- Right-click the Alarm and Event Log Viewer object and then clickProperties.
Use the
Toolbar
tab in the FactoryTalk Alarm and Event Log Viewer Properties dialog box to change the buttons that are displayed on the toolbar in the Alarm and Event Log Viewer at runtime.The following table describes the settings available on the
Toolbar
tab and how they can be used:Setting | Description |
---|---|
Add and remove toolbar buttons | The toolbar buttons at the top of the Alarm and Event Log Viewer provide quick access to operations for operators. Add or remove the toolbar buttons as needed. |
Reposition toolbar buttons | To move the button name up or down in the list, click a button name in the list, and then click the Move Up or Move Down buttons. |
Change toolbar button captions | To change the caption for a button, select the button name in the Caption list and then in the text box, type a caption for the button.If the caption is not visible on the button, select a different format for the button in the Format list. |
Change toolbar button tooltips | To change the tooltip for a button, select the button in the Tooltip list, and then, in the text box, type a tooltip for the button. |
Display images, captions, or both on toolbar buttons | To change how a button is displayed on the toolbar, select the button in the Format list and then select one of the available formats. |
Provide Feedback