Alarm and Event Log Viewer Properties - Columns tab
How do I open the Alarm and Event Log Viewer Properties dialog box?
To open the
FactoryTalk Alarm and Event Log Viewer Properties
dialog box at design time:- OpenFactoryTalk ViewStudio.
- Add anAlarm and Event Log Viewerobject to a graphic display.
- Right-click the Alarm and Event Log Viewer object and then clickProperties.
Use the
Columns
tab in the FactoryTalk Alarm and Event Log Viewer Properties
dialog box at design time to change the columns displayed in the Alarm and Event Log Viewer at runtime.The following table describes the settings available on the
Columns
tab and how they can be used:Setting | Description |
---|---|
Add and remove columns in the event list | The columns across the top of the event list represent some of the data fields in the Alarm and Event Log Viewer. All of the data fields are shown in the details pane, but you can select the ones you want to display in the event list. |
Reposition columns | To change the order in which columns are displayed in the event list, click a column name in the list, and then click the Move Up or Move Down buttons to move the column name up or down in the list. |
Change column headings | To change the heading of a column, select the column name in the Heading text list and then type a name in the text box.This name is displayed in the heading for the column in the event list and in the details pane. The text you type in the text box does not replace the original name of the column in the column list, or on the Display Filter tab. |
Change column widths | To change the width of columns in the event list, select the column name in the Width list, and then type a number in the text box.For example, increase the width of the column if you expect the text in the column to be long or vice versa. |
Change column alignment | In the Align list, select the alignment in which you want the information to appear in the column. |
Change the format of information displayed in columns | In the Format list, select the format in which you want the information to appear in the column.
|
Show seconds for all timestamps | To define the timestamps at runtime, click and select the timestamp type from the drop-down list box: Show seconds for all timestamps , Show milliseconds for all timestamps , and Show microseconds for all timestamps . |
Provide Feedback