User Rights Assignment Policy Properties
How do I open User Rights Assignment Policy Properties?
- StartFactoryTalk Administration ConsoleorFactoryTalk View Studioand then log on to theFactoryTalkNetwork Directory orFactoryTalkLocal Directory.
- InExplorer, expand theFactoryTalkNetwork or Local Directory tree, and then expand theSystem>Policies>System Policiesfolders.
- SelectUser Rights Assignment.
In
User Rights Assignment Policy Properties
, specify which users are permitted to:- Switch between primary and secondary servers in a redundant pair (for example, HMI servers, or data servers)
Policy settings are completely separate in the network directory and local directory. The network directory and local directory also have different default policy settings.
Provide Feedback