Modify Security Authority Identifier

How do I open Modify Security Authority Identifier?
  • In
    FactoryTalk Administration Console
    , select
    Tools > FactoryTalk Security Authority Identifier
    .
Use
Modify Security Authority Identifier
to generate, back up, or restore the unique Security Authority Identifier for a
FactoryTalk Directory
. The
User Rights Assignment > Modify Security Authority Identifier
permission is required to generate, back up, or restore the identifier.
Secure controller projects and controllers running secure projects can only be accessed when the
FactoryTalk Directory
Security Authority identifier matches the identifier saved in the project. This prevents unauthorized access to a controller or controller project if moved or copied to a different
FactoryTalk Directory
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal