Generate a Security Authority identifier
Each
FactoryTalk Directory
has a unique Security Authority identifier generated during installation. Generate a Security Authority identifier to change the Security Authority identifier assigned to the FactoryTalk Directory
.Secure controller projects and controllers running secure projects can only be accessed when the
FactoryTalk Directory
Security Authority identifier matches the identifier saved in the project. This prevents unauthorized access to a controller or controller project if moved or copied to a different FactoryTalk Directory
.
IMPORTANT:
After generating a new Security Authority identifier, controllers and controller projects secured with the previous identifier cannot be accessed.
Prerequisites
- Obtain the following permissions fromSystem > System Policies> User Rights Assignment:
- UseLogix Designerto remove security from any controllers and controller projects in theFactoryTalk Directory.
- Shut down allFactoryTalksoftware products, components, and services exceptFactoryTalk Administration Console.
To generate a Security Authority identifier
- InFactoryTalk Administration Console, selectTools >.FactoryTalkSecurity Authority Identifier
- InModify Security Authority Identifier, selectGenerate ID.
- In the confirmation window, select Yes.
- (optional) selectBackupto back up the current directory with the new identifier.
- SelectClose.
- Sign in to FactoryTalk.IMPORTANT: You must sign in to FactoryTalk after a new Security Identifier is generated to enable the changes. Selectto view the new Security Identifier.Tools > FactoryTalk Authority Security Identifier...
- (optional) UseLogix Designerto add security to any controllers and controller projects in theFactoryTalk Directory.
Provide Feedback