Configure Securable Action

How do I open Configure Securable Action?
  1. In
    FactoryTalk Administration Console
    Explorer
    , expand the
    System
    >
    Policies >
    Product Policies
    .
  2. Expand the product folder, then right-click
    Feature Security
    and select
    Properties
    .
  3. In
    Feature Security Properties
    , select the row containing the feature category.
  4. Next to
    Configure Security
    , select
    Browse
    (
    ...
    ).
Use
Configure Securable Action
to view or set the permissions that determine access to a single feature for a user or group of users working from a computer or group of computers connected to the
FactoryTalk
network directory. The product policy features that can be secured depend on what
FactoryTalk
products are installed.
Use this window to configure permissions for the actions in
User Rights and Assignment Properties
.
In a
FactoryTalk
local directory, all security settings apply to only the local computer.
Setting
Description
Permissions list
Shows the users and computers that have
Allow
or
Deny
permissions set for this feature.
To allow access to the feature, select
Allow
.
To deny access to the feature, select
Deny
.
If both
Allow
and
Deny
are cleared, the user is denied access to the feature.
Add
Select to add users and computers to the permissions list to set explicit permissions.
Remove
In the permissions list, select the combination of users and computers for which to remove security settings, and select
Remove
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal