Configure SMTP policy
Configure the SMTP policy to use an SMTP server for sending email notifications from FactoryTalk-enabled software.
Prerequisites
Configure an SMTP server.
To configure the SMTP policy
- In FactoryTalk Administration Console or FactoryTalk View StudioExplorer, expandSystem > Policies > System Policies.
- Right-clickSMTP Policy, and then selectProperties.
- InSMTP Policy Properties, configure the following:
- SMTP server domain name or IP address.
- Port number. The default is 25.
- Select the authentication type used by the SMTP server.
- (optional) Sender's email address.
- Enable encrypted communication with the SMTP server.
- Test the connection by selectingTest SMTP.
- InTest Connection, enter a recipient's email address, and then selectTest.
- SelectOK.
Provide Feedback