SMTP Policy Properties
- In FactoryTalk Administration Console or FactoryTalk View StudioExplorer, expandSystem > Policies > System Policies.
- Right-clickSMTP Policy, and then selectProperties.
Configure the SMTP policy to use an SMTP server for sending email notifications from FactoryTalk-enabled software.
Use these properties to configure the SMTP policy.
Setting | Description |
---|---|
SMTP Server Address | Sets the SMTP server domain name or IP address that is used for delivering notification emails. |
Port | Sets the communication port for the SMTP server. The default is 25. |
Log in | Sets the authentication type.
|
"From" email address | Sets the optional sender's email address.
|
The SMTP Server requires a secure connection (TLS). | Turns on the encrypted communication between the SMTP server and the SMTP client. TLS 1.2 and TLS 1.3 are supported. |
Test SMTP | Tests the current SMTP server configuration. |
Provide Feedback