Authorize an application to access the FactoryTalk Directory
Use to authorize applications to access the
FactoryTalk
Service Application Authorization FactoryTalk Directory
.The option to verify the publisher certificate information is enabled by default, applications that are not signed by
Rockwell Automation
or Microsoft®
are not allowed access to the FactoryTalk Directory
.
TIP:
To configure the
Application Authorization
policy, log into FactoryTalk
with an account that is a member of the FactoryTalk
Administrators group.To authorize an application to access the
FactoryTalk Directory
- Log on to theFactoryTalknetwork directory orFactoryTalklocal directory.
- InFactoryTalk Administration ConsoleExplorer, expand theSystem>Policies>System Policiesfolders.
- Right-clickApplication Authorizationand selectProperties.TheApplication Authorizationpolicy controls access by monitoring information about each application that is requesting a service token fromFactoryTalk.
- In, review the list of the applications that can be authorized. To sort the application list by process name, computer name, or access allowed status, select the corresponding column header at the top of the window.FactoryTalkService Application AuthorizationSome applications are required byFactoryTalkand cannot be removed or denied. These entries are displayed with gray text in the list.
- (optional) To view the publisher certificate information for a process, select the desired cell in thePublisher Infocolumn.
- Select a process, and then scroll to the right to view its access status. SelectAccess Allowedto provide access to theFactoryTalk Directory, or clear to deny access to theFactoryTalk Directory.
- (optional) To automatically enable access to theFactoryTalk Directoryfor any new process, selectEnable Default Access.
- (optional) To automatically block access to theFactoryTalk Directoryfor any new process, clearEnable Default Access.
- (optional) To allow applications that are not signed, clearVerify Publisher Info.
- SelectOK.
Provide Feedback