Allow a resource to inherit permissions
Permissions determine which users can perform which actions on specific resources in the system from which computers. Set
Allow
and Deny
permissions on resources. Allow a resource to inherit permissions when the selected resource has the same permissions as its parent resource. For example, if assigning security to an area in an application, all of the items in the area inherit the security settings of the area. By default, the area inherits security settings from the application. The top of the hierarchy is the network directory or local directory.
To allow a resource to inherit permissions
- InFactoryTalk Administration ConsoleExplorer, right-click the resource, then selectSecurity.
- InSecurity Settings, on thePermissionstab, clearDo not inherit permissions.
- To remove explicit permissions, clear the black check mark next toAlloworDeny. Inherited permissions appear as gray check marks and cannot be removed. However, explicit permissions supersede inherited permissions.
- SelectOK.TIP:Security settings configured for resources apply to allFactoryTalkproducts in the system in the currentFactoryTalkdirectory. For example, if a user and computer are deniedReadaccess to an area, that user and computer cannot see the area in any of theFactoryTalkproducts in the system.
Provide Feedback