Configure a permission set

Permission sets identify a set of actions that are allowed or denied for one or more user groups or computer groups. Create a permission set to apply the same set of permissions to multiple controllers or project components in a
Logix Designer
application.
After creating a permission set, secure it by setting permissions for user-computer pairs.
To configure a permission set
  1. Expand the
    System
    folder and
    Permission Sets
    folder.
  2. Right-click the permission set to secure and select
    Security
    .
  3. In
    Security Settings
    , configure permissions for a user-computer pair. A pair can include groups as well as individual users and computers.
  4. Select
    OK
    .
Open the
Logix Designer
application. The new permission set appears in the
Permission Sets
menu and can be applied to projects and project components.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal