Set the syslog policy for a computer group
The syslog configurations in
FactoryTalk
are managed system-wide in System Policies
. Use these configurations to modify:
- Syslog collector settings
- Message buffering
- Message categories
Some circumstances require overriding the default system-wide settings and specifying the syslog policy for a specific group of computers. If a computer group has the syslog policy disabled, the syslog policy of computers in the computer group will be disabled and cannot be modified. If a computer group has the syslog policy enabled, you can modify the syslog policy of computers in the computer group as needed. More information about how to set the syslog system policy for a computer, refer to Set the syslog policy for a computer.
Prerequisites
Setting the syslog system policy for a computer group requires these permissions:
- Common > List Children
- Common > Read
- Common > Write
- Common > Configure Security
- InFactoryTalk Administration ConsoleExplorer, expandSystem > Computers and Groups > Computers Groups.
- Right-click the computer, and then selectProperties.
- Select theDiagnosticstab.
- Enable or disable syslog forwarding for the computer group.
- SelectApply.
Provide Feedback