Select Computer Group

How do I open Select Computer Group?
  1. Navigate to either
    New Computer
    or
    Computer Properties.
  2. In the
    General
    tab, click
    Add
    .
After adding a computer to the
FactoryTalk
network directory, add the computer to a computer group to have the computer inherit the security settings of the group.
Use
Select Computer Group
to:
  • Select one or more computer group accounts that the currently selected computer account should be added to.
  • Create a new computer group and then add it to the computer's group memberships.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal