New Area
How do I open New Area?
- InFactoryTalk Administration ConsoleExplorer, right-click a network application, then selectNew Area.
Use areas to organize and subdivide a distributed network application into logical or physical divisions. Example: Create separate areas that correspond with separate manufacturing lines in a facility, separate plants in different geographical locations, or different manufacturing processes.
Areas are not available with local applications.
Enter these settings to identify the new area.
Setting | Description |
---|---|
Name (required) | In the Name box, type a descriptive name to identify the area. Area name rules:
|
Description (optional) | In the Description box, enter text to describe the area to its users. Examples: Geographic location, the type of equipment, the operator group, technical support contact information, or software version history. |
Provide Feedback