Add an area
Areas organize and subdivide a distributed network application into logical or physical divisions. Example: Create areas for different processes within a manufacturing facility. To use multiple HMI servers in a single application, create a new area for each HMI server.
Areas can be created within existing areas. Areas are not supported in local applications.
Prerequisites
Adding areas requires these permissions:
- Common > Create Children
- Common > List Children
- Common > Read
To add an area
- InFactoryTalk Administration ConsoleExplorer, expand theNetworktree.
- Right-click the application or area, and then selectNew Area.
- Type a name and optional description for the area, and then selectOK.
Provide Feedback