The right FactoryTalk Directory is not configured on this computer
The correct
FactoryTalk
Directory may not be installed on your computer, or the administrator account that allows access to that directory may be disabled if the following occurs:- Attempting to log on to aFactoryTalkLocal Directory orFactoryTalkNetwork Directory but are not allowed access.
- Installing aFactoryTalkproduct and experiencing unexpected error messages when running the product.
To correct this problem, go to
Rockwell Software > FactoryTalk Tools
and run FactoryTalk Directory Configuration Wizard
.Provide Feedback